covarTD(numX,numY,x1,t1,x2,t2,…,xN,tN,y1,s1,y2,s2,…,yM, sM)

covarTD(numX,numY,x1,t1,x2,t2,…,xN,tN,y1,s1,y2,s2,…,yM, sM)

This transform generates a cross covariance matrix (numX columns each of length numY) with time delays (row number shifts). numX and numY are the numbers of X and Y variables. x1,t1,… is a list of X variables each with a time delay (number of rows); y1,s1,… is a list of Y variables each with a time delay. The X and Y variables must be numeric. This special transform requires up to numX output variable names, as described in “Transforms With Multiple Outputs”.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal