atand(x) or atand(y,x)

atand(x) or atand(y,x)

Arctangent, result in degrees. Like atan, this function can take one or two arguments. For one argument, the result is between -90 and +90; for two arguments, the result is between -179.9999… and +180.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal