changestat($self,startrow,[endrow,]status)

changestat($self,startrow,[endrow,]status)

This transform is used to change the status of one or more rows in a single column to any of “Blank”, “Break”, “Cut”, “Error”, “OK”. If endrow is omitted, it is assumed to be the same as startrow. The status names are not case-sensitive. See also forcestat(x,status).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal