clearRows($self,startrow[,endrow])

clearRows($self,startrow[,endrow])

Changes the variable's status in the specified row(s) to Blank. The arguments are a variable of any type, and one or two row numbers. If the endrow is omitted, it defaults to be the same as the startrow. The output variable must be the same as the input.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal