fmt(x,format)

fmt(x,format)

Builds a string by writing a numeric value according to the specified format. The format is specified as “w.r”, where w is the width of the output string and r is the number of places printed to the right of the decimal point. For example, $fmt(123.4567,'5.2') returns the string 123.45. The output is a string variable.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal