scatcut(Yvar-self,[Ylow,Yhigh,]Xvar,Xlow,Xhigh,startrow,en drow)

scatcut(Yvar-self,[Ylow,Yhigh,]Xvar,Xlow,Xhigh,startrow,en drow)

Within the specified row number range, this transform cuts points from the Y variable (not from X) when both Xvar and Yvar fall within the specified range of values. The output variable must be the same as the input Y variable. (This transform is not currently attached to a plot action.)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal