iifft(realVar,imagVar,length)

iifft(realVar,imagVar,length)

This function takes as input two variables that are interpreted as real and imaginary values, and an FFT length that is a constant power of 2, and returns a single real column that is the raw inverse FFT.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal