sort(var1,var2[,direction])

sort(var1,var2[,direction])

This function takes as input two variables and an optional direction. It sorts the second column in the order of the first column, in either ascending or descending order. The direction is the constant $ascend or $descend, and defaults to $ascend if omitted.
NOTE:
This Transform cannot be translated by Data Explorer into a streaming equivalent.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal