differs(var)

Takes as input a variable of any type; returns 1 if the value in the current row is different from the value in the previous row, and 0 if they are the same. If the current row has any bad status, the result is Error; if the current row has a good status but the previous row has a bad status, the result is 1.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.