System-Generated Transforms

System-Generated Transforms

These transform functions are generated automatically from user actions. When these functions have been applied to a dataset, they appear in the Transform List and you can delete or modify them, as necessary. You can also type them directly into the Transform Window.
IMPORTANT:
If you perform an action that generates one of these transforms, and then you want to rescind that action, you should delete the transform, rather than performing an opposite action that generates another transform; for example, delete a Cut instead of applying an Uncut.
Unless specified otherwise, the input variables can be of any type.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal