Applied from Plots

Applied from Plots

Cuts and Clips are implemented as transforms. If you apply them from plots or from the context menu, the transform is generated automatically. You can edit or delete a Cut or Clip, just like any other transform. In the specifications that follow, startrow and endrow are starting and ending row numbers; low and high are a range of the variable's values; dtVal is a date/time constant in the format \mm/dd/yy hh:mm:ss\.
clipabove($self,value) or clipbelow($self,value)
: For the specified variable, it changes any value above or below the given value to equal the value. The output variable must be the same as the input.
cutabove($self,value) or cutbelow($self,value)
: For the specified variable, it cuts any point above or below the given value. The output variable must be the same as the input.
markcut($self,startrow,endrow[,low,high])
: The generated version of this transform omits the optional low and high values and simply cuts within the specified range of rows. You can edit the transform to further limit the cut to the specified range of values. The output variable must be the same as the input.
timecut($self,dtVal1,dtVal2[,low,high])
: The generated version of this transform omits the optional low and high values and simply cuts within the specified range of time. You can edit the transform to further limit the cut to the specified range of values. The output variable must be the same as the input.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal