Enable FactoryTalk Design Studio Copilot - Project Access

Enable FactoryTalk Design Studio Copilot - Project Access

FactoryTalk Design Studio
Project Access
is a Core entitlement feature that enables
FactoryTalk Design Studio
Copilot's project search and code generation capabilities.
Project Access
is disabled by default.
To enable FactoryTalk Design Studio Project Access
  1. Select
    File > Options
    .
  2. Select
    Copilot
    .
  3. In
    Copilot
    , toggle
    Project Access
    to
    On
    .
For more information about the
FactoryTalk Design Studio
Copilot, see FactoryTalk Design Studio Copilot.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.