- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Toolbar
Icons in the toolbar include:
Icon | Description |
---|---|
![]() | Devices list . Opens the Devices list to view and set controller and device properties. |
![]() | Commit . Save changes to the local repository. |
![]() | Push . Transfer commits from the local repository for the shared project to the remote repository. The number in the icon identifies the total commits made by the current user (local commits). |
![]() | Pull . Update the local repository of the shared project from the remote repository. The number in the icon identifies the total commits made by other users sharing the project (remote commits). |
![]() | The Change history tab shows all changes committed to the repository for a local or shared project. |
Provide Feedback