- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Go online or offline with a controller
On the Online pane, use the Online-Offline toggle to go online or offline with a controller.
TIP:
You can be online with only one controller at a time.
To go online or offline with a controller
- From the right-hand panel, selectOnlineto open the Online pane.
- In the Online pane, select theOnline-offlineicon
to go online or offline with a controller.
If errors occur while going online, check the View messages and status with the Output pane for messages.
Provide Feedback