- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Monitor controller status
Use the Online pane to monitor controller status.
These status indicators appear on the Online pane:

Object | Description |
---|---|
![]() | Online-Offline toggle. The toggle is green when the controller is online. Slide the toggle to the right to go online with a controller. Slide it to the left to go offline with a controller. A yellow triangle above the toggle indicates a warning: ![]() A red circle above the toggle indicates a fault or error, and the Controller mode indicates the controller is in a fault state: ![]() |
![]() | Key switch or toggle switch position on the physical controller. If the physical controller's key switch or toggle switch is set to REM (Remote), you can use FactoryTalk Design Studio or the Logix Designer application to change the controller mode. If the controller mode switch is set to RUN or PROG, you cannot change the controller mode from FactoryTalk Design Studio or the Logix Designer application. |
![]() | Current controller mode:
|
![]() | Controller LED lights:
|
For more information on controller status messages, refer to these sources:
Provide Feedback