- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
File Sort (SRT)
The SRT instruction sorts a set of values in one dimension (Dim to vary) of the array into ascending order.
IMPORTANT:
You must test and confirm that the instruction does not change data that you don’t want it to change.
If you specify an array that is a member of a structure, and the length exceeds the size of that array you must test and confirm that the SRT instruction does not change data you do not want changed.
The data is constrained by the specified member.
In this transitional instruction, the relay ladder toggles the rung-condition-in from false to true for the instruction to execute.
Available Languages
Ladder Diagram
_v1.png/_jcr_content/renditions/original)
FactoryTalk Design Studio
DSL - Ladder DiagramSRT(Array,Dimtovary,Control);
Operands
Ladder Diagram
Operand | Type | Format | Description |
---|---|---|---|
Array | SINT INT DINT REAL | Array tag | array to sort specify the first element of the group of elements to sort |
Dimension to vary | DINT | Immediate (0, 1, 2) | which dimension to use the order of the dimensions is: array[0,1,2] |
Control | CONTROL | Tag | control structure for the operation |
Length | DINT | Immediate | number of elements of the array to sort |
Position | DINT | Immediate | current element in the array initial value is typically 0 |
CONTROL Structure
Mnemonic | Data Type | Description |
---|---|---|
.EN | BOOL | The enable bit indicates the SRT instruction is enabled. |
.DN | BOOL | The done bit is set when the instruction has operated on the last element in the Array. |
.ER | BOOL | The error bit is set when either .LEN < 0 or .POS < 0. Either of these conditions also generates a major fault. When .ER bit is set, the instruction does not execute. |
.LEN | DINT | The length word specifies the number of elements in the array on which the instruction operates. |
.POS | DINT | The position word identifies the current element that the instruction is accessing. |
Affects Math Status Flags
No
Major/Minor Faults
A major fault will occur if: | Fault type | Fault code |
---|---|---|
.POS < 0 or .LEN < 0 | 4 | 21 |
Dimension to vary > number of dimensions | 4 | 20 |
Length > end of array | 4 | 20 |
See Common Attributes for operand related faults.
Execution
Ladder Diagram
Condition / State | Action Taken |
---|---|
Prescan | N/A. |
Rung-condition-in is false | .EN bit is cleared to false .EN bit is cleared to false .DN bit is cleared to false |
Rung-condition-in is true | The instruction executes |
Postscan | N/A. |
Examples
Example 1
Sort DINT_array, which is DINT[4,5].

Ladder Diagram

Example 2
Sort DINT_array, which is DINT[4,5].
(10).png/_jcr_content/renditions/original)
Ladder Diagram

Provide Feedback