Protect graphic objects with a password
Protect a container or a drawing with a password to prevent other
FactoryTalk Optix Studio
users from editing the protected object children.
IMPORTANT:
Protecting graphic objects with a password may not prevent advanced users from bypassing the object protection and should not be considered a safety or intellectual property protection.
- InProject view, right-click a container or drawing object to protect.
- Select.
- Enter a password.
- (optional) SelectShow passwordto verify that you entered the password correctly.
- SelectOK.
In
appears next to the password protected object. The child objects are hidden in
Project view
and in the Editor
, ![](/content/dam/dita/en/factorytalk-optix/current/_images/password-protected-locked.png/_jcr_content/renditions/original)
Project view
and cannot be edited.Provide Feedback