Unlock graphic objects protected with a password
Unlock a password protected graphic object to view and edit its child objects.
- InProject viewor in theEditor, next to the object to unlock, select.
- Enter the password and selectOK.
In
appears next to the password protected object. You can view and edit unlocked object child objects.
Project view
and in the Editor
, ![](/content/dam/dita/en/factorytalk-optix/current/_images/password-protected-unlocked.png/_jcr_content/renditions/original)
Provide Feedback