Deployment
Compile your
FactoryTalk Optix Application
for your client devices and then run them.Prerequisites
- To compile a, the client device on which the application runs must be configured inFactoryTalk Optix ApplicationFactoryTalk Optix Studio. See Configure a client device
- To deploy and run the application the client device must haveand a valid license. If the client device is unlicensed, the application runs in demo mode, which means that it stops running after two hours.FactoryTalk Optix Application Update Service
- InFactoryTalk Optix Studio, selectStopto stop any currently running on the client device
Set the active client device
The client device that
FactoryTalk Optix Studio
can connect to on the network to automatically deploy the compiled application is defined as active
. From FactoryTalk Optix Studio
, you can also stop the execution of the application on the active and linked client device.To set a client device as active, expand and then select the desired client device.
TIP:
Automatic run after a project is deployed is supported by default on
Rockwell Automation
client devices. Either manual run or automatic startup must be configured for other client devices. If the client device is already running a FactoryTalk Optix Application
, FactoryTalk Optix Studio
stops it before deploying another application.Provide Feedback