Subscription-based Runtime entitlements

FactoryTalk Optix Runtime supports non-perpetual entitlements, that you can activate like any other entitlement.
The grace period lasts seven days before expiration, during which you receive a daily notification about the number of days remaining in the grace period.
  • If you do not activate any new entitlement prior to the grace period expiration, Runtime becomes available in demo mode only and can run for two hours.
    NOTE: You can allocate an entitlement while Runtime runs in demo mode. However you need to manually restart Runtime to activate the new entitlement.
  • If you activate an entitlement during the grace period, the grace period ends.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.