Develop a temperature change alarm

Develop an alarm that signals when temperature exceeds a set value.
Application example
NOTE:
Download a sample project:
TemperatureChangeAlarm.zip
Prerequisites
  1. To develop the project
  2. Arrange the interface elements.
  3. Save the project.
Application design example
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.