Develop a localized event logger
Create an even logger that displays the interface in the language of a currently logged-in user.
NOTE:
Download a sample project:
LocalizedEventLogger.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Select to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback