Develop a solution that samples and stores data

Create an application that samples the value of a variable on the value change and stores that data in an embedded database.
Application example
NOTE:
Download a sample project:
SampleStoreDataValueChange.zip
Prerequisites
  1. To develop the project
  2. In
    Project view
    , right-click
    Model
    and select
    New
    Variable
    .
  3. Create a data logger with an embedded database that monitors the value change of the variable. See Add a data logger.
  4. Arrange the interface elements.
  5. Save the project.
Application design example
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.