Develop a button that changes label text

Develop a button that changes the text of a label when you select the button.
Application example
TIP:
You can download a sample project from:
ButtonThatChangesLabelText.zip
Prerequisites
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.