Develop a solution for importing translations

Use OPC UA communication to import translations from another project.
Application example - client, login form
Application example - client, logged in Italian user
Application example - client, logged-in American user
NOTE:
Download a sample project:
ImportTranslations.zip
Prerequisites
TIP: The Client project imports data from the Server project.
  1. To develop the server project
  2. Arrange the interface elements.
  3. Save the project.
  4. To develop the client project
  5. Arrange the interface elements.
  6. Save the project.
Application design example
Select
Run
to run server and client projects using the client emulator to test your project. To run the projects on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.