Develop a UI that generates a PDF report
Generate a PDF report with a custom header and footer that contains information from a data grid.
NOTE:
Download a sample project:
PDFReportWithDataGrid.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Select to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback