Develop a confirmation dialog

Create a confirmation dialog that displays when you select a button. This project involves the creation of a custom method invocation.
Application example - save dialog
Application example - apply value dialog
NOTE:
Download a sample project:
DialogConfirmation.zip
Prerequisites
Application design example - confirmation dialog
Application design example - save panel
Application design example - value panel
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.