Develop a button that animates an SVG image
Configure an Advanced SVG Image object to animate the image at runtime.
NOTE:
Download a sample project:
RotateImage.zipPrerequisites
- To develop the project
- Arrange the interface elements.
Select to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Run
Provide Feedback