Develop automatically generated UI

Develop a UI populated automatically with graphical elements based on the properties of objects in the Model folder.
NOTE:
Download a sample project:
UIGeneratedFromModel.zip
Example application
Prerequisites
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.