Function Block Editor Sheet toolbar
The Function Block Editor includes a toolbar to help you do common tasks. Tooltips on the toolbar indicate the intended use of each tool. Move your cursor over the icons to see the tooltips.
Use this toolbar to:
- Toggle between Original, Pending Edits, or Test Edits view.
- Add or insert new sheets.
- Delete existing sheets.
- Change the order of sheets.
- Navigate between previous and next sheets.
- Show/hide grid lines.
- Navigate to a sheet using sheet number.
- Add sheet descriptions.
Provide Feedback