Patch deployment cancel
Local connection: Use FTUpdater to collect detailed information for a local network. FTUpdater provides screens and export to view your software inventory and usage. Another way to consume the data is by connection to the database. With an OBDC driver, connect to the FTUpdater Server database
C:\ProgramData\Rockwell\Updater\Data\Server.DB
. A workflow to view Server.DB tables in Excel is shown below. Multiple connections: To scale up beyond a single network or a production line to a production site to a collection of sites, data must be aggregated. Aggregating data from several databases can be accomplished with analytics tools such PowerBi.
Provide Feedback