Air Gap automated patch deployment
FactoryTalk Updater v4.10 allows automated air gapped deployment of Monthly Patch Rollups to multiple computers. Communication between these system is by file transfers. The files require password encryption as they are exported and decryption as they are imported.
Provide Feedback