Use IT Mode to retrieve information and download patches for OT software
Use IT mode to obtain the latest information and to download the latest patches for the installed software exported from OT mode.
IT mode only supports downloading patches, not deploying patches.
TIP:
IT mode differs from Normal mode. In IT mode, it is not possible to manage groups. Additionally, these features are unavailable: Find Machines, Schedule, and Activations.
- SelectImport software list.
- Search for the.zipfile that contains the OT software list. SelectOpen.
- Enter the password for the.zipfile. SelectOK.The software list is imported. The latest version and latest patch information appear.
- Select.
- In theSave towindow, selectBrowse.
- In theSave Aswindow, type the name of the exported file, and selectSave.
- Enter a password for the file.
- Confirm the password and selectOK.
- To download the patch, select the product.
- Sign in to PCDC.
- SelectDownload.
- Accept the EULA.
- Select the location.
- Copy the patch and the exported IT software list (.zipfile) to the OT file server.
Provide Feedback