Import updated Zip file from IT mode into OT mode
Once you retrieve the latest software information and patches from PCDC by using IT mode, import the updated Zip file and patches into OT mode.
TIP:
To deploy patches and information, the FT Updater client must connect to FactoryTalk Updater server with an administrator user account.
- Import the data from the saved.zipfile by selectingUpdate Database.
- Select the exported IT list.
- Enter the password and selectOK.The last patch and version is imported.
- Select the products that you want to deploy, and selectDeploy.
- In theDeploy Patcheswindow, browse for the patch.
- Determine when to install the patch.
- Determine when to restart the computer after installing the patch.
- SelectDeploy.The patch roll-up uploads to the server and then distributed to the agents.
Provide Feedback