Export the OT mode software list to a Zip file

When you are working in an OT environment, use the OT mode to manage Rockwell Automation software on the agent. Since an OT environment is disconnected from the Internet, OT mode is dependent on the IT mode to obtain the latest information and patches. 
From OT mode, export the software list to a server or USB flash drive. From either location, paste the software list to the IT environment.
  1. From the menu, select
    Export
    Software list
    .
  2. In the
    Save to
    window, select
    Browse
    .
  3. In the
    Save As
    window, type the name of the exported file, and select
    Save
  4. Enter a password for the file.
  5. Confirm the password and select
    OK
    .
  6. Copy the exported
    .zip
    file to the IT environment file server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.