- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Configure the appearance and behavior of Logix Designer
These topics describe how to configure the appearance and behavior of the
Logix Designer
application. Follow the instructions to customize the application to suit your needs.
TIP:
If
FactoryTalk Security
is enabled, the Trends
tab on the Workstation Options
dialog may be unavailable, depending on the levels of access that have been defined.Provide Feedback