Dashboards

Asset Intelligence Dashboards

Dashboard Introduction
In Asset Intelligence, the dashboard section of the application is where all users are able to interact with the associated KPI’s, Alerts and trending data, that is all contextualized by the asset and hierarchical location.
Users are able to see rolled-up KPI status based on the hierarchy, see overview of each element of the hierarchy, and be able to determine where they need to focus their efforts in addressing various alerts within the application.
This section of the User Manual will go through each key level of the hierarchy and what the application provides, as well as the different types of alerts, how they function and how a user would interact with them.
Hierarchy Dashboard Items
The following are the list of alerts available in the application:
  • KPI Alerts
  • Sensor Fault Alerts
  • Advisory Alerts
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal