Sub-area level dashboard

Sub-Area Level Dashboard

In this dashboard, you can view the configured hierarchy lists. Based on the configuration, respective KPI details are displayed in the
Overview
tab in the form of cards.
Select the required sub-area from the hierarchy list and you can see the following tabs in the dashboard:
  1. Overview
  2. Assets
Overview
tab:
You can view the bullet chart of the configured KPI parameters under the selected sub-area and the top five underperforming assets in the selected time frame. You can also view the active alerts with severity, actions taken, and the current status of the alert.
Summary chart
NOTE: Click the [>], [>>], [<], [<<] paginator icons in the summary graph to move forward and backward to view the data.
In the KPI trend chart, three lines indicate the three different KPI data, the solid lines indicate the historical data, and the dotted line indicates the extrapolated future projected data.
When you click over the dotted line, you can see the red color dotted line that indicates the alert threshold line.
Threshold Chart
You can view the individual KPI graph of the top 5 underperforming assets and the graph is shown for the past 3 months.
Top 5 underperforming assets
NOTE: You can use the [] in the respective column to filter based on your needs.
Click the [] icon on the left side of the respective asset name to view the asset hierarchy details.
Asset hierarchy details
You can view all the active alerts with alert descriptions, severity, start date, action taken, and current status details.
Active alerts
To change the time period, click the [] icon and select the required date in the
From
and
To
box.
Assets
tab:
You can view summaries of the asset classes associated to this point in the hierarchy. Each card represents an Asset Class with rolled-up statuses. By selecting an individual Asset Class, you can filter the list of assets available in the
Asset Details
section.
Asset cards
Asset details
NOTE: Click on any cards from the summary section to view the relevant asset class in the asset details section.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal