- Extractors
- Analyze Data
Delete Application
- On the Management Console, select theApplicationstab.The applications list is displayed.
- In theActionscolumn, click the Delete icon next to the application that you want to delete.The selected application's detail page is displayed.
- ClickDelete Applicationto proceed deleting the application.NOTE:Deleting an application removes all the information including the client secret. The application can no longer be used for viewing data from FactoryTalk DataMosaix. Before deleting an application, verify the information so that you delete the correct application.TheConfirm Deletiondialog box is displayed.
- ClickDelete.The application is removed from the applications list.
Provide Feedback