Edit Application

Edit Application

  1. On the Management Console, select the
    Applications
    tab.
    The
    Applications Listing
    page is displayed.
    Applications Listing
  2. In the
    Actions
    column, click the Edit icon next to the application that you want to edit.
    Edit Icon
    The selected application's detail page is displayed.
    You can edit the application information such as App Name, Application URL, and Description.
  3. Edit the information in the required fields.
  4. Click
    Save Changes
    .
    The
    Applications
    tab displays the updated information for the edited application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal