Configure the Associated Axes and Control Mode
After you associate the axis to the drive, configure the axis and control mode.
To configure the Associated Axes and Control mode:
- From theAxis Propertiesdialog box, inCategories, clickGeneral.
- In theGeneralarea, from theAxis Configurationlist, select the axis configuration type.TIP:The availableAxis Configurationvalues are determined by the drive's profile and the default selection. If there is no drive associated with the axis, all values are available, and the default position isPosition Loop.
- From theFeedback Configurationlist, select the feedback configuration type.TIP:TheFeedback Configurationvalues vary by profile and axis type.
- From theApplication Typelist, select the application type.
- From theLoop Responselist, select the desired loop response.
- ClickApply.
Provide Feedback