Drive is permitting motor torque while the safety controller is in Program Mode

The CIP safety drive associated with this axis is currently permitting motor torque while the safety controller is in Program Mode. This occurs when a Motion Direct Command is issued to a drive where the Safe Torque Off function has been bypassed.
If you want to perform the Motion Direct Command, click
Yes
. If you want to cancel the Motion Direct Command, click
No
. The dialog box closes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.