PLLS status and commands

Use the
General
tab on the
PLLS Properties
dialog box to monitor the instruction status and issue online commands to Process Lead Lag Standby Motor Group (PLLS) instructions.
Monitor the instruction status and issue online commands for PLLS instructions
  1. On the instruction in the routine, perform one of these actions:
    • On the Ladder or FBD instruction, select .
    • In the Structured Text editor, right-click the tag name and select
      Configure <tag name>
      .
  2. Select these commands when online with the controller.
    • Bypassable permissives & interlocks: Check
      . Tells the instruction that all permissives and interlocks, bypassable or not, are to be checked during operation.
    • Bypassable permissives & interlocks: Bypass
      . Tells the instruction that bypassable permissives and interlocks are bypassed, or ignored, during operation.
    • Operator/Maintenance online commands
      :
      The action is immediate if the command request does not need to be confirmed by the operator. If the command request requires a signature, this will enforce security from the HMI and disable the command from the Logix Designer dialog.
      • Start
        . Start the motor group.
      • Stop
        . Stop the motor group.
    • Sheds and alarms reset
      . Reset all sheds and alarms of the instruction. The button is enabled when the device and the instruction are ready for reset and a signature is not required. The action is immediate if the command request does not need to be confirmed by the operator. If the command request requires a signature, this will enforce security from the HMI and disable the command from the Logix Designer dialog. The button is always disabled when the device is offline.
  3. When online with the controller, monitor the
    Device state
    and
    Device issues
    indicators at the bottom left of the dialog box:
    • Device state
      . Displays the current device state:
      • None
      • Stopped
      • Running
      • Stopping
      • Decreasing
      • Increasing
    • Device issues
      . Displays fault conditions:
      • None
      • Configuration error
      • Fail to start
      • Fail to stop
  4. Monitor the values and current states for permissives, interlocks, and sheds.
  5. Select
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.