PVSD datalinks
Use the
Datalinks
tab of the PVSD Properties
dialog box to monitor datalinks for the Process Variable Speed Drive (PVSD) instruction. To monitor datalinks for PVSD instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select .
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Select the arrow next toGeneraland then selectDatalinks.
- Set the parameter:
- Output datalink operator setting. Type a value for the output datalink to use in operator mode. If the setting requires a signature, this will enforce security from the HMI and disable the setting from the Logix Designer dialog.
- View the read-only parameters:
- Numeric values. Displays the current value of the input, configuration, or output.
- Device state. When theLogix Designerapplication is online with the controller, the indicator displays the current device state, such as Stopped, Running, or Out of service.
- Device issues. When theLogix Designerapplication is online with the controller, the indicator displays fault conditions, such as Drive fault or I/O fault.
Provide Feedback