Verification Steps (Application Installation)

Verification Steps (Application Installation)

Perform the following steps to verify that the application is successfully installed:
  1. Ensure that the following services are running:
    1. FTASecurity
    2. FactoryTalk Activation Helper
    3. FactoryTalk Activation Service
    4. FactoryTalk Activation WebsocketService
    5. PostgreSQL
    6. Elasticsearch
    7. FTAnalyticsDataImporter
    8. FTAnalyticsDataView
  2. Open the URL
    https://<FQDN-hostname>/dataview
    using a web browser to open the DataView application.
    TIP:
    The login URL for DataView should match with the ‘Valid Redirect URI’ entered in the Security Provider.
    Login Page
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.