Import Users

Import Users

  1. Log in to DataView with admin credentials. The Admin console page displays.
    DataView Admin Console
  2. Navigate to the Manage Users menu.
  3. Select [Import Users].
  4. In the Import Users page, search for the list of Users that have not been imported into DataView. This list should include the User dvuser created earlier.
  5. Under the Select User column, select the User to import (for example: user2).
  6. Select [Design User] from the Select Role drop-down list.
    Select Users
  7. Click [Import].
    Import Users
    The “User imported successfully” message displays.
  8. After the successful update, the dvuser can now use the DataView application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.