Delete Role
NOTE:
You can delete the Roles in both list and detail view.
Perform the following steps to update the Role:
- Click [Administration] on the left navigation panel.
- Select the Roles tab, the list of the Roles displays.
- Select the checkboxes of the Role(s) in the list which you want to delete.
- Click the [
] icon on the top right corner and click [Delete].
Delete Role - The ‘Delete Role(s)’ dialog displays, click [Delete].Confirm Delete
Provide Feedback