HMI navigation for PBL
Use the
HMI Navigation
tab of the PBL Properties
dialog box to enable or disable navigation from the HMI to input and output objects.To enable HMI navigation to input and output objects for PBL instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Under theHMItab, selectNavigation.
- To allow navigation to the input and output object from the HMI faceplate, selectAllow navigation.
- In theObject tag namebox, enter the name of the object.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device state depending on the value of the Out_Live parameter. Use theHMItab to enter text in theText to display when output equals 0andText to display when output equals 1boxes.
- Device issues. Displays fault conditions:None, orConfiguration error.
- SelectApply.
Provide Feedback