Monitor Input and Output gates for Process Boolean Logic (PBL) instructions
Use the
PBL Properties
dialog box - General
tab to monitor the Input and Output gates on Process Boolean Logic (PBL) instructions.
TIP:
Use the
Advanced - Input gate
and Output gate
tabs to configure gate settings.To monitor Input and Output gates for Process Boolean Logic (PBL) instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Monitor this information for the eight Input gates and the Output gate.
- Input label. The inputs for the gate.
- Function. The function configured for the gate. Functions include AND, OR, XOR, M out of N, Set-Reset (latch), and Select (switch gate).
- Value. The current numeric value of the input or output.
- Inversion status. A circle appears for inputs that are inverted.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device state depending on the value of the Out_Live parameter. Use theHMItab to enter text in theText to display when output equals 0andText to display when output equals 1boxes.
- Device issues. Displays fault conditions:None, orConfiguration error.
- SelectApply.
Provide Feedback