PBL timers, time stamps, snapshots
Use the
Advanced
tab on the PBL Properties
dialog box to configure timestamps, overwrite settings, and triggering conditions for snapshots.Configure timers, time stamps, and snapshots for Process Boolean Logic (PBL) instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Select theAdvancedtab.
- Configure these settings:
- Generate a controller timestamp when snapshot occurs. Select this checkbox to enable a timestamp on each snapshot. The timestamp is based on the controller clock setting.A snapshot captures the state of the instruction, including all input states, gate states, and output states for later use. Use snapshots for evaluating logic after a shutdown for capturing the state of the logic when it trips or shuts down equipment. This includes instances when the logic states change after the shutdown.
- Allow a new snapshot to overwrite an existing snapshot without a snapshot reset. Select this checkbox to allow a new snapshot to trigger before the previous snapshot is reset.
- Save state to snapshot when. Select conditions that trigger a snapshot:
- Hold input transitions from 0 to 1
- Output transitions from 0 to 1
- Output transitions from 1 to 0
- Requested by operator (enables snapshot button)
- Requested by program command
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device state depending on the value of the Out_Live parameter. Use theHMItab to enter text in theText to display when output equals 0andText to display when output equals 1boxes.
- Device issues. Displays fault conditions:None, orConfiguration error.
- SelectApply.
Provide Feedback